- Thu Apr 29, 2021 11:54 am
#225455
I've been making a ton of progress on a project using an Artemis DK and mBed Studio. But at some point over the last 24 hours, the serial monitor stopped printing messages from the dev kit.
I can definitely update the code on the board (verified by changing LED blink rate). I haven't yet tried to see if I can receive data over the USB serial connection.
Environment is macOS 10.15.17, mBed Studio 1.4.0.2, mBed OS 6.10, and using the mbed_os_blinky_example program (with an added printf). I've set the baud rate of the Serial Monitor to 9600, which is what it was set to when things were previously working.
I should add that I also don't see any output when I directly cat the USB serial port.
I can definitely update the code on the board (verified by changing LED blink rate). I haven't yet tried to see if I can receive data over the USB serial connection.
Environment is macOS 10.15.17, mBed Studio 1.4.0.2, mBed OS 6.10, and using the mbed_os_blinky_example program (with an added printf). I've set the baud rate of the Serial Monitor to 9600, which is what it was set to when things were previously working.
I should add that I also don't see any output when I directly cat the USB serial port.