- Sat Nov 18, 2023 11:35 am
#245338
I am trying to use the Sno M2 with the Input & Display carrier board. I can run GetXLR8Version just fine, as well as the Blink example. But when I try run the test sketch for the display I get nothing. I have made sure that I have all 3 of the required libraries installed and there are no errors when uploading the Example1_DisplayTest sketch to the Sno M2.
I noticed on the Input & Display Hookup Guide https://learn.sparkfun.com/tutorials/sp ... okup-guide that the Sno M2 is not shown under the "Required Materials" section. Does that mean it is not supported? Would it be possible to get the two working together, even if it is difficult?
I noticed on the Input & Display Hookup Guide https://learn.sparkfun.com/tutorials/sp ... okup-guide that the Sno M2 is not shown under the "Required Materials" section. Does that mean it is not supported? Would it be possible to get the two working together, even if it is difficult?