- Thu Apr 20, 2023 9:32 am
#240542
Hello World
Revisiting an old project of mine (lost my notes so half starting from square 1). I have the MicroMod Weather board with an ESP32 processor board. Couldn't remember why I had an external BME280 installed when there's one right there on the board. Figured it out, the on-board BME280 seems to be consistently reading inaccuratly on all fronts compared to the QWIIC connected BME280:
Revisiting an old project of mine (lost my notes so half starting from square 1). I have the MicroMod Weather board with an ESP32 processor board. Couldn't remember why I had an external BME280 installed when there's one right there on the board. Figured it out, the on-board BME280 seems to be consistently reading inaccuratly on all fronts compared to the QWIIC connected BME280:
Code: Select all
Based on other commercial sensors in the area the QWIIC connected BME is reading more accurately than the on-board BME280. Is this because I'm using an ESP32 for the processor (generating heat)? The devices are on different addresses, code is literally 1:1 the same for reading either sensor.Temperature: 60.49
Humidity: 44
Pressure: 98722
Altitude: 718.3
On-board Temperature: 68.59
On-board Humidity: 34
On-board Pressure: 98756
On-board Altitude: 708.8