- Wed Feb 22, 2023 6:25 pm
#239234
2.4" TFT Input and display carrier board with an ESP32 processor board
I can make several peripherals out on the QWIIC bus work and can make the push-button example code work. So I'm thinking that I'm loading libraries correctly, have the right board configuration, and everything is working. I just don't see anything on the display when I try to run any of the "HyperDisplay 4DLCD-320240" example code options. The display backlight is on, but there is nothing on display. I've tried loading the code with a MicroSD card installed, and without a MicroSD card installed. (Do I have to pre-format the MicroSD card or something?) None of the tutorials mention anything about needing a MicroSD card to get the example code to work. What am I missing?
I can make several peripherals out on the QWIIC bus work and can make the push-button example code work. So I'm thinking that I'm loading libraries correctly, have the right board configuration, and everything is working. I just don't see anything on the display when I try to run any of the "HyperDisplay 4DLCD-320240" example code options. The display backlight is on, but there is nothing on display. I've tried loading the code with a MicroSD card installed, and without a MicroSD card installed. (Do I have to pre-format the MicroSD card or something?) None of the tutorials mention anything about needing a MicroSD card to get the example code to work. What am I missing?