- Fri Mar 01, 2024 12:14 pm
#247608
Hi,
For the life of me, I cannot get two Artemis RedBoard to talk to each other over I2C and I don't understand why.
I have stripped everything from the boards the only connections I have are (top right of the board, near the USBC connector)
Controller Target
-------------- ---------
SCL <------------------> SCL
SDA <------------------> SDA
GND <------------------> GND
I uploaded the code from [the Arduino doc](https://docs.arduino.cc/learn/communication/wire/)
Controller:
I am not seeing anything on the serial terminal. These are the signals that I see on the I2C bus (blue is SCL, yellow is SDA): I have tested the exact same code between two esp32 and everything works as expected.
I don't understand what I am doing wrong.
For the life of me, I cannot get two Artemis RedBoard to talk to each other over I2C and I don't understand why.
I have stripped everything from the boards the only connections I have are (top right of the board, near the USBC connector)
Controller Target
-------------- ---------
SCL <------------------> SCL
SDA <------------------> SDA
GND <------------------> GND
I uploaded the code from [the Arduino doc](https://docs.arduino.cc/learn/communication/wire/)
Controller:
Code: Select all
Target:
// Wire Controller Reader
// by Nicholas Zambetti [http://www.zambetti.com](http://www.zambetti.com)
// Demonstrates use of the Wire library
// Reads data from an I2C/TWI peripheral device
// Refer to the "Wire Peripheral Sender" example for use with this
// Created 29 March 2006
// This example code is in the public domain.
#include <Wire.h>
void setup() {
Wire.begin(); // join i2c bus (address optional for master)
Serial.begin(9600); // start serial for output
}
void loop() {
Wire.requestFrom(8, 6); // request 6 bytes from peripheral device #8
while (Wire.available()) { // peripheral may send less than requested
char c = Wire.read(); // receive a byte as character
Serial.print(c); // print the character
}
delay(500);
}
Code: Select all
// Wire Peripheral Sender
// by Nicholas Zambetti [http://www.zambetti.com](http://www.zambetti.com)
// Demonstrates use of the Wire library
// Sends data as an I2C/TWI peripheral device
// Refer to the "Wire Master Reader" example for use with this
// Created 29 March 2006
// This example code is in the public domain.
#include <Wire.h>
void setup() {
Wire.begin(8); // join i2c bus with address #8
Wire.onRequest(requestEvent); // register event
}
void loop() {
delay(100);
}
// function that executes whenever data is requested by master
// this function is registered as an event, see setup()
void requestEvent() {
Wire.write("hello "); // respond with message of 6 bytes
// as expected by master
}
I am not seeing anything on the serial terminal. These are the signals that I see on the I2C bus (blue is SCL, yellow is SDA): I have tested the exact same code between two esp32 and everything works as expected.
I don't understand what I am doing wrong.
You do not have the required permissions to view the files attached to this post.