- Wed Oct 07, 2020 4:17 am
#219542
Dear Sparkfun,
Recently got a Sparkfun DEV-16832
And a Sparkfun GPS-15712
These are connected via a 50mm Qwiic cable. Both boards have red LED illuminated, the GPS board has flashing Blue LED illuminated.
The Firmware on DEV-16832 is set to OpenLog_Artemis-V10-v16.bin
A USB-C cable connects to the Sparkfun DEV-16832 board using a Hyperterminal set at 115kbaud, pressing the reset button the unit reports following details at boot,
D init failed (second attempt). Is card present? Formatted?
Config file read failed: SD offline
Artemis OpenLog v1.6
ICM-20948 failed to init.
SD card offline
Datalogging offline
Serial logging offline
IMU offline
Identifying Qwiic Devices...
Autodetect complete
Device config file read failed: SD offline
GPS-ublox online at address 0x42
It can see the attached GPS board, and GPS co-ordinates are streaming and displayed at 100Hz rate but doesn’t seem to recognize the onboard IMU and temperature sensors and at boot it reports its IMU chip ICM-20948 is offline.
From the main menu option 3 shows the IMU logging and all IMU sensors are enabled but can’t see any IMU data in data stream viewing on Hyper terminal.
Grateful if you can advise how to enable the IMU logging on this device, thank you.
Regards,
Nick
Recently got a Sparkfun DEV-16832
And a Sparkfun GPS-15712
These are connected via a 50mm Qwiic cable. Both boards have red LED illuminated, the GPS board has flashing Blue LED illuminated.
The Firmware on DEV-16832 is set to OpenLog_Artemis-V10-v16.bin
A USB-C cable connects to the Sparkfun DEV-16832 board using a Hyperterminal set at 115kbaud, pressing the reset button the unit reports following details at boot,
D init failed (second attempt). Is card present? Formatted?
Config file read failed: SD offline
Artemis OpenLog v1.6
ICM-20948 failed to init.
SD card offline
Datalogging offline
Serial logging offline
IMU offline
Identifying Qwiic Devices...
Autodetect complete
Device config file read failed: SD offline
GPS-ublox online at address 0x42
It can see the attached GPS board, and GPS co-ordinates are streaming and displayed at 100Hz rate but doesn’t seem to recognize the onboard IMU and temperature sensors and at boot it reports its IMU chip ICM-20948 is offline.
From the main menu option 3 shows the IMU logging and all IMU sensors are enabled but can’t see any IMU data in data stream viewing on Hyper terminal.
Grateful if you can advise how to enable the IMU logging on this device, thank you.
Regards,
Nick