I tried it at home today and I see these logs at the end when the logging stops and the OLA kind of disconnects (means I can no longer use the console input).
Where is the code for the Qwiic button you are mentioning @PaulZC?
Here is what I get in the log:
Code: Select allAutodetect complete
waitForQwiicBusPowerDelay: qwiicPowerHasBeenOnFor 15660ms
beginQwiicDevices: attempting to begin deviceType Particle-SNGCJA5 at address 0x33 using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType ADC-ADS1015 at address 0x48 using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType ADC-ADS1015 at address 0x49 using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType ADC-ADS1015 at address 0x4A using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType ADC-ADS1015 at address 0x4B using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType Qwiic_Button at address 0x6F using mux address 0x0 and port number 0
beginQwiicDevices: device is online
beginQwiicDevices: attempting to begin deviceType Pressure-MS5837 at address 0x76 using mux address 0x0 and port number 0
beginQwiicDevices: device is online
setMaxI2CSpeed: setting qwiic clock speed to 100000Hz
Particle-SNGCJA5 online at address 0x33
ADC-ADS1015 online at address 0x48
ADC-ADS1015 online at address 0x49
ADC-ADS1015 online at address 0x4A
ADC-ADS1015 online at address 0x4B
Qwiic_Button online at address 0x6F
Pressure-MS5837 online at address 0x76
Device count: 7