- Thu Sep 15, 2022 9:58 am
#235815
I have new Artemis OpenLogger with latest 2.4 firmware. The unit works fine, but after about 3 hours, it simply stops loggging to the SD Card, which is not nearly full. I am logging from the gps and temperature recorder that came with the kit and logging at the fastest rate, which with GPS and temp logger is about 4 Hz.
I removed a lot of data from the midsection of the log file to make it small enough to send. It looks like the logger logged about an hour and 6 minutes worth of data and quit. The two bright LEDs and the quickly flashing little green LED we blinking as normal , but it stopped logging to SD card. The first time I tried it, the logger logged only about 3 minutes and stopped logging.
I removed a lot of data from the midsection of the log file to make it small enough to send. It looks like the logger logged about an hour and 6 minutes worth of data and quit. The two bright LEDs and the quickly flashing little green LED we blinking as normal , but it stopped logging to SD card. The first time I tried it, the logger logged only about 3 minutes and stopped logging.
You do not have the required permissions to view the files attached to this post.