- Sat Feb 12, 2011 10:44 pm
#120137
This is a slightly "Arduino-ified" version of the previous code, which allows the nrf24ap1 to get the information from a Garmin HR strap, and process the data with an 3.3v Arduino. Note that it uses the SoftwareSerial library to talk to the ANT receiver, so that the standard serial ports are free to communicate with a computer. This allows me to use the heartrate info to control things on my computer, like the volume of VLC player. I do that with another python script that reads the other end of the serial connection.
Code: Select all
#include <SoftwareSerial.h>
#define UCHAR unsigned char
#define rxPin 2
#define txPin 3
#define ledPin 13
// set up a new serial port
SoftwareSerial mySerial = SoftwareSerial(rxPin, txPin);
byte pinState = 0;
#define RETURN_ERROR -1
#define RETURN_SUCCESS 0
#define DEBUG 1
#define MESG_TX_SYNC ((UCHAR)0xA4)
#define MESG_RX_SYNC ((UCHAR)0xA5)
#define MESG_SIZE_OFFSET ((UCHAR)1)
#define MESG_ID_OFFSET ((UCHAR)2)
#define MESG_SYNC_SIZE ((UCHAR)1)
#define MESG_SIZE_SIZE ((UCHAR)1)
#define MESG_ID_SIZE ((UCHAR)1)
#define MESG_CHECKSUM_SIZE ((UCHAR)1)
#define MESG_MAX_DATA_SIZE ((UCHAR)17)
#define MESG_HEADER_SIZE (MESG_SYNC_SIZE + MESG_SIZE_SIZE + MESG_ID_SIZE)
#define MESG_DATA_OFFSET MESG_HEADER_SIZE
#define MESG_FRAME_SIZE (MESG_HEADER_SIZE + MESG_CHECKSUM_SIZE)
#define MESG_MAX_SIZE (MESG_MAX_DATA_SIZE + MESG_FRAME_SIZE)
//////////////////////////////////////////////
// Message ID's
//////////////////////////////////////////////
#define MESG_INVALID_ID ((UCHAR)0x00)
#define MESG_EVENT_ID ((UCHAR)0x01)
#define MESG_VERSION_ID ((UCHAR)0x3E) // protocol library version
#define MESG_RESPONSE_EVENT_ID ((UCHAR)0x40)
#define MESG_UNASSIGN_CHANNEL_ID ((UCHAR)0x41)
#define MESG_ASSIGN_CHANNEL_ID ((UCHAR)0x42)
#define MESG_CHANNEL_MESG_PERIOD_ID ((UCHAR)0x43)
#define MESG_CHANNEL_SEARCH_TIMEOUT_ID ((UCHAR)0x44)
#define MESG_CHANNEL_RADIO_FREQ_ID ((UCHAR)0x45)
#define MESG_NETWORK_KEY_ID ((UCHAR)0x46)
#define MESG_RADIO_TX_POWER_ID ((UCHAR)0x47)
#define MESG_RADIO_CW_MODE_ID ((UCHAR)0x48)
#define MESG_SEARCH_WAVEFORM_ID ((UCHAR)0x49)
#define MESG_SYSTEM_RESET_ID ((UCHAR)0x4A)
#define MESG_OPEN_CHANNEL_ID ((UCHAR)0x4B)
#define MESG_CLOSE_CHANNEL_ID ((UCHAR)0x4C)
#define MESG_REQUEST_ID ((UCHAR)0x4D)
#define MESG_BROADCAST_DATA_ID ((UCHAR)0x4E)
#define MESG_ACKNOWLEDGED_DATA_ID ((UCHAR)0x4F)
#define MESG_BURST_DATA_ID ((UCHAR)0x50)
#define MESG_CHANNEL_ID_ID ((UCHAR)0x51)
#define MESG_CHANNEL_STATUS_ID ((UCHAR)0x52)
#define MESG_RADIO_CW_INIT_ID ((UCHAR)0x53)
#define MESG_CAPABILITIES_ID ((UCHAR)0x54)
#define MESG_NVM_DATA_ID ((UCHAR)0x56)
#define MESG_NVM_CMD_ID ((UCHAR)0x57)
#define MESG_NVM_STRING_ID ((UCHAR)0x58)
#define MESG_ID_LIST_ADD_ID ((UCHAR)0x59)
#define MESG_ID_LIST_CONFIG_ID ((UCHAR)0x5A)
#define MESG_OPEN_RX_SCAN_ID ((UCHAR)0x5B)
#define MESG_EXT_CHANNEL_RADIO_FREQ_ID ((UCHAR)0x5C)
#define MESG_EXT_BROADCAST_DATA_ID ((UCHAR)0x5D)
#define MESG_EXT_ACKNOWLEDGED_DATA_ID ((UCHAR)0x5E)
#define MESG_EXT_BURST_DATA_ID ((UCHAR)0x5F)
#define MESG_CHANNEL_RADIO_TX_POWER_ID ((UCHAR)0x60)
#define MESG_GET_SERIAL_NUM_ID ((UCHAR)0x61)
#define MESG_GET_TEMP_CAL_ID ((UCHAR)0x62)
#define MESG_SET_LP_SEARCH_TIMEOUT_ID ((UCHAR)0x63)
#define MESG_SET_TX_SEARCH_ON_NEXT_ID ((UCHAR)0x64)
#define MESG_SERIAL_NUM_SET_CHANNEL_ID_ID ((UCHAR)0x65)
#define MESG_RX_EXT_MESGS_ENABLE_ID ((UCHAR)0x66)
#define MESG_RADIO_CONFIG_ALWAYS_ID ((UCHAR)0x67)
#define MESG_ENABLE_LED_FLASH_ID ((UCHAR)0x68)
#define MESG_AGC_CONFIG_ID ((UCHAR)0x6A)
#define MESG_READ_SEGA_ID ((UCHAR)0xA0)
#define MESG_SEGA_CMD_ID ((UCHAR)0xA1)
#define MESG_SEGA_DATA_ID ((UCHAR)0xA2)
#define MESG_SEGA_ERASE_ID ((UCHAR)0XA3)
#define MESG_SEGA_WRITE_ID ((UCHAR)0XA4)
// ((UCHAR)0xA5) //FREE
#define MESG_SEGA_LOCK_ID ((UCHAR)0xA6)
#define MESG_FUSECHECK_ID ((UCHAR)0xA7)
#define MESG_UARTREG_ID ((UCHAR)0XA8)
#define MESG_MAN_TEMP_ID ((UCHAR)0xA9)
#define MESG_BIST_ID ((UCHAR)0XAA)
#define MESG_SELFERASE_ID ((UCHAR)0XAB)
#define MESG_SET_MFG_BITS_ID ((UCHAR)0xAC)
#define MESG_UNLOCK_INTERFACE_ID ((UCHAR)0xAD)
#define MESG_IO_STATE_ID ((UCHAR)0xB0)
#define MESG_CFG_STATE_ID ((UCHAR)0xB1)
#define MESG_RSSI_ID ((UCHAR)0xC0)
#define MESG_RSSI_BROADCAST_DATA_ID ((UCHAR)0xC1)
#define MESG_RSSI_ACKNOWLEDGED_DATA_ID ((UCHAR)0xC2)
#define MESG_RSSI_BURST_DATA_ID ((UCHAR)0xC3)
#define MESG_RSSI_SEARCH_THRESHOLD_ID ((UCHAR)0xC4)
#define MESG_BTH_BROADCAST_DATA_ID ((UCHAR)0xD0)
#define MESG_BTH_ACKNOWLEDGED_DATA_ID ((UCHAR)0xD1)
#define MESG_BTH_BURST_DATA_ID ((UCHAR)0xD2)
#define MESG_BTH_EXT_BROADCAST_DATA_ID ((UCHAR)0xD3)
#define MESG_BTH_EXT_ACKNOWLEDGED_DATA_ID ((UCHAR)0xD4)
#define MESG_BTH_EXT_BURST_DATA_ID ((UCHAR)0xD5)
//////////////////////////////////////////////
// Message Sizes
//////////////////////////////////////////////
#define MESG_INVALID_SIZE ((UCHAR)0)
#define MESG_RESPONSE_EVENT_SIZE ((UCHAR)3)
#define MESG_CHANNEL_STATUS_SIZE ((UCHAR)2)
#define MESG_VERSION_SIZE ((UCHAR)9)
#define MESG_UNASSIGN_CHANNEL_SIZE ((UCHAR)1)
#define MESG_ASSIGN_CHANNEL_SIZE ((UCHAR)3)
#define MESG_CHANNEL_ID_SIZE ((UCHAR)5)
#define MESG_CHANNEL_MESG_PERIOD_SIZE ((UCHAR)3)
#define MESG_CHANNEL_SEARCH_TIMEOUT_SIZE ((UCHAR)2)
#define MESG_CHANNEL_RADIO_FREQ_SIZE ((UCHAR)2)
#define MESG_NETWORK_KEY_SIZE ((UCHAR)9)
#define MESG_RADIO_TX_POWER_SIZE ((UCHAR)2)
#define MESG_RADIO_CW_MODE_SIZE ((UCHAR)3)
#define MESG_RADIO_CW_INIT_SIZE ((UCHAR)1)
#define MESG_SEARCH_WAVEFORM_SIZE ((UCHAR)3)
#define MESG_SYSTEM_RESET_SIZE ((UCHAR)1)
#define MESG_OPEN_CHANNEL_SIZE ((UCHAR)1)
#define MESG_CLOSE_CHANNEL_SIZE ((UCHAR)1)
#define MESG_REQUEST_SIZE ((UCHAR)2)
#define MESG_CAPABILITIES_SIZE ((UCHAR)6)
#define MESG_DATA_SIZE ((UCHAR)9)
#define MESG_NVM_DATA_SIZE ((UCHAR)10)
#define MESG_NVM_CMD_SIZE ((UCHAR)3)
#define MESG_NVM_STRING_SIZE ((UCHAR)9)
#define MESG_ID_LIST_ADD_SIZE ((UCHAR)6)
#define MESG_ID_LIST_CONFIG_SIZE ((UCHAR)3)
#define MESG_OPEN_RX_SCAN_SIZE ((UCHAR)1)
#define MESG_EXT_CHANNEL_RADIO_FREQ_SIZE ((UCHAR)3)
#define MESG_EXT_DATA_SIZE ((UCHAR)13)
#define MESG_RADIO_CONFIG_ALWAYS_SIZE ((UCHAR)2)
#define MESG_RX_EXT_MESGS_ENABLE_SIZE ((UCHAR)2)
#define MESG_SET_TX_SEARCH_ON_NEXT_SIZE ((UCHAR)2)
#define MESG_SET_LP_SEARCH_TIMEOUT_SIZE ((UCHAR)2)
#define MESG_SERIAL_NUM_SET_CHANNEL_ID_SIZE ((UCHAR)3)
#define MESG_ENABLE_LED_FLASH_SIZE ((UCHAR)2)
#define MESG_GET_SERIAL_NUM_SIZE ((UCHAR)4)
#define MESG_GET_TEMP_CAL_SIZE ((UCHAR)4)
#define MESG_AGC_CONFIG_SIZE ((UCHAR)2)
#define MESG_READ_SEGA_SIZE ((UCHAR)2)
#define MESG_SEGA_CMD_SIZE ((UCHAR)3)
#define MESG_SEGA_DATA_SIZE ((UCHAR)10)
#define MESG_SEGA_ERASE_SIZE ((UCHAR)0)
#define MESG_SEGA_WRITE_SIZE ((UCHAR)3)
#define MESG_SEGA_LOCKED_SIZE ((UCHAR)1)
#define MESG_SEGA_LOCK_SIZE ((UCHAR)0)
#define MESG_FUSECHECK_SIZE ((UCHAR)1)
#define MESG_UARTREG_SIZE ((UCHAR)2)
#define MESG_MAN_TEMP_SIZE ((UCHAR)2)
#define MESG_BIST_SIZE ((UCHAR)6)
#define MESG_SELFERASE_SIZE ((UCHAR)2)
#define MESG_SET_MFG_BITS_SIZE ((UCHAR)2)
#define MESG_UNLOCK_INTERFACE_SIZE ((UCHAR)1)
#define MESG_IO_STATE_SIZE ((UCHAR)2)
#define MESG_CFG_STATE_SIZE ((UCHAR)2)
#define MESG_RSSI_SIZE ((UCHAR)3)
#define MESG_RSSI_DATA_SIZE ((UCHAR)17)
#define MESG_RSSI_SEARCH_THRESHOLD_SIZE ((UCHAR)2)
#define RETURN_ERROR -1
#define RETURN_SUCCESS 0
#define DEBUG 1
// Ant Stuff
#define MAXMSG 14 // SYNC,LEN,MSG,data[8],CHKSUM
#define CHAN0 0
#define CHAN1 1
#define NET0 0
#define NET1 1
#define TIMEOUT 10 //mikec 30
#define BAUD 4800 // Sparkfun ANT Default Baud
//#define FREQ 0x41; // Suunto radio frequency
#define FREQ 0x39; // garmin radio frequency
//#define PERIOD 0x199a; // Suunto search period
#define PERIOD 0x1f86; // Garmin search period
//#define NETWORK_KEY "B9AD3228757EC74D" // Suunto HRM
#define NETWORK_KEY "B9A521FBBD72C345" // Garmin HRM
// Macros
#define hexval(c) ((c >= '0' && c <= '9') ? (c-'0') : ((c&0xdf)-'A'+10))
#define TRUE 1
#define FALSE 0
#if !defined(NULL)
#define NULL ((void *) 0)
#endif
#define MAX_UCHAR 0xFF
#define MAX_SCHAR 0x7F
#define MIN_SCHAR 0x80
#define MAX_SHORT 0x7FFF
#define MIN_SHORT 0x8000
#define MAX_USHORT 0xFFFF
#define MAX_SSHORT 0x7FFF
#define MIN_SSHORT 0x8000
#define MAX_LONG 0x7FFFFFFF
#define MIN_LONG 0x80000000
#define MAX_ULONG 0xFFFFFFFF
#define MAX_SLONG 0x7FFFFFFF
#define MIN_SLONG 0x80000000
// GLOBAL VARIABLES
///////////////////
UCHAR rxBuf[MAXMSG];
UCHAR checkSum(UCHAR *data, int length)
{
int i;
UCHAR chksum = data[0];
for (i = 1; i < length; i++)
chksum ^= data[i]; // +1 since skip prefix sync code, we already counted it
return chksum;
}
int hstr2hex(UCHAR *hex, char *hexstr, int size)
{
int i;
if ((size % 2) != 0)
{
Serial.println("hstr2hex error: input hex string has to be divisible by 2");
exit(RETURN_ERROR);
}
for (i=0; i < (size/2); i++)
{
hex[i] = hexval(hexstr[i*2])*16 + hexval(hexstr[i*2 + 1]);
}
return RETURN_SUCCESS;
}
//ANT_send(1+1, MESG_SYSTEM_RESET_ID, 0x00)
// Resets module
void reset (void)
{
uint8_t i;
uint8_t buf[4];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x01; // LENGTH Byte
buf[2] = MESG_SYSTEM_RESET_ID; // ID Byte
buf[3] = 0x00; // Data Byte N (N=LENGTH)
buf[4] = checkSum(buf,4);
Serial.print("TX: ");
for(i = 0 ; i < 5 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
//ANT_send(1+2, MESG_REQUEST_ID, CHAN0, MESG_CAPABILITIES_ID)
void assignch(void)
{
uint8_t i;
uint8_t buf[5];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x02; // LENGTH Byte
buf[2] = MESG_REQUEST_ID; // ID Byte
buf[3] = CHAN0; //
buf[4] = MESG_CAPABILITIES_ID; //
buf[5] = checkSum(buf,5);
Serial.print("TX: ");
for(i = 0 ; i < 6 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
// ANT_send(1+2, MESG_REQUEST_ID, CHAN0, 0x3D)
void assignch1(void)
{
uint8_t i;
uint8_t buf[5];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x02; // LENGTH Byte
buf[2] = MESG_REQUEST_ID; // ID Byte
buf[3] = CHAN0; //
buf[4] = ((UCHAR)0x3D); //
buf[5] = checkSum(buf,5);
Serial.print("TX: ");
for(i = 0 ; i < 6 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
// ANT_send(1+3, MESG_ASSIGN_CHANNEL_ID, CHAN0, 0x00, NET0); // chan, chtype (0=wildcard?), network
void assignch2(void)
{
uint8_t i;
uint8_t buf[6];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x03; // LENGTH Byte
buf[2] = MESG_ASSIGN_CHANNEL_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = ((UCHAR)0x00);
buf[5] = NET0;
buf[6] = checkSum(buf,6);
Serial.print("TX: ");
for(i = 0 ; i < 7 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
// ANT_send(1+5, MESG_CHANNEL_ID_ID, CHAN0, 0x00, 0x00, 0x00, 0x00); // chan, devno (2byte) (0=wildcard) (little-endian), devtype (0=wildcard), manid (0=wildcard));
void assignch3(void)
{
uint8_t i;
uint8_t buf[8];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x05; // LENGTH Byte
buf[2] = MESG_CHANNEL_ID_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = ((UCHAR)0x00);
buf[5] = ((UCHAR)0x00);
buf[6] = ((UCHAR)0x00);
buf[7] = ((UCHAR)0x00);
buf[8] = checkSum(buf,8);
Serial.print("TX: ");
for(i = 0 ; i < 9 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
// MESG_NETWORK_KEY_ID, net1, GARMIN_KEY
// buf[0] = MESG_NETWORK_KEY_ID;
// buf[1] = NET0;
// hstr2hex(&buf[2], NETWORK_KEY, 16); // dest, orig, size
// ANT_sendStr(1+9, buf);
void assignch4(void)
{
uint8_t i;
uint8_t buf[12];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x09; // LENGTH Byte
buf[2] = MESG_NETWORK_KEY_ID; // ID Byte
buf[3] = NET0;
hstr2hex(&buf[4], NETWORK_KEY, 16); // dest, orig, size
//mikec hstr2hex(&buf[2], NETWORK_KEY, 16); // dest, orig, size
buf[12] = checkSum(buf,12);
Serial.print("TX: ");
for(i = 0 ; i < 13 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
//ANT_send(1+2, MESG_CHANNEL_SEARCH_TIMEOUT_ID, CHAN0, TIMEOUT); // MESG_CHANNEL_SEARCH_TIMEOUT_ID, chan, timeout);
void timeout(void)
{
uint8_t i;
uint8_t buf[5];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x02; // LENGTH Byte
buf[2] = MESG_CHANNEL_SEARCH_TIMEOUT_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = TIMEOUT;
buf[5] = checkSum(buf,5);
Serial.print("TX: ");
for(i = 0 ; i < 6 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
//ANT_send(1+2, MESG_CHANNEL_RADIO_FREQ_ID, CHAN0, FREQ);
void frequency(void)
{
uint8_t i;
uint8_t buf[5];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x02; // LENGTH Byte
buf[2] = MESG_CHANNEL_RADIO_FREQ_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = FREQ;
buf[5] = checkSum(buf,5);
Serial.print("TX: ");
for(i = 0 ; i < 6 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
//ANT_send(1+3, MESG_CHANNEL_MESG_PERIOD_ID, CHAN0, PERIOD%256, PERIOD/256); // NOTE: Period = Little-endian
void channel_period(void)
{
uint8_t i;
uint8_t buf[6];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x03; // LENGTH Byte
buf[2] = MESG_CHANNEL_MESG_PERIOD_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = 0x1f; //mikec buf[4] = 0x9A;
buf[5] = 0x86; //mikec buf[5] = 0x19; // 6554 = 25*256 + 154; 25=0x19; 154 = 0x9A
buf[6] = checkSum(buf,6);
Serial.print("TX: ");
for(i = 0 ; i < 7 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
//ANT_send(1+1, MESG_OPEN_CHANNEL_ID, CHAN0); // MESG_OPEN_CHANNEL_ID, chan
void open_channel(void)
{
uint8_t i;
uint8_t buf[4];
buf[0] = MESG_TX_SYNC; // SYNC Byte
buf[1] = 0x01; // LENGTH Byte
buf[2] = MESG_OPEN_CHANNEL_ID; // ID Byte
buf[3] = CHAN0;
buf[4] = checkSum(buf,4);
Serial.print("TX: ");
for(i = 0 ; i < 5 ; i++)
{
Serial.print(buf[i], HEX);
Serial.print(" ");
mySerial.print(buf[i]);
}
Serial.println("");
}
void config (void)
{
Serial.println("Config Starting");
reset();
delay(100);
assignch();
delay(1000);
assignch1();
delay(100);
assignch2();
delay(100);
assignch3();
delay(100);
assignch4();
delay(20);
timeout();
delay(20);
frequency();
delay(20);
channel_period();
delay(20);
open_channel();
delay(20);
Serial.println("Config Done");
}
int ANT_rxHandler()
{
int n, fd, rc, inmsg = FALSE;
UCHAR chr, msgN;
while (mySerial.available()>0)
{
chr = mySerial.read();
if (chr == -1)
{
Serial.println("Unknown error has occured");
}
else
{
if ((chr == MESG_TX_SYNC) && (inmsg == FALSE))
{
msgN = 0; // Always reset msg count if we get a sync
inmsg = TRUE;
rxBuf[msgN] = chr; // second byte will be msg size
msgN++;
Serial.println("RX: [sync]");
}
else if (msgN == 1)
{
rxBuf[msgN] = chr; // second byte will be msg siz
msgN++;
// Serial.print("..0x");
// Serial.print(chr,HEX);
}
else if (msgN == 2)
{
rxBuf[msgN] = chr;
msgN++;
// Serial.print("..0x");
// Serial.print(chr,HEX);
}
else if (msgN < rxBuf[1]+3) // sync, size, checksum x 1 byte
{
rxBuf[msgN] = chr;
msgN++;
// Serial.print("..0x");
// Serial.print(chr,HEX);
}
else
{
inmsg = FALSE;
rxBuf[msgN] = chr;
// Serial.print("..0x");
// Serial.println(chr,HEX);
if (checkSum(rxBuf, msgN) == rxBuf[msgN]) // Check if chksum = msg chksu
{
// Serial.print("RX: msg received-");
// Serial.println(msgN);
ANT_rxMsg();
}
else
{
Serial.println("RX: chksum mismatch");
}
}
}
}
}
int ANT_rxMsg()
{
//int i;
UCHAR msgID, msgSize;
UCHAR *msgData;
// copy args
// memcpy(rxBuf, args, sizeof(UCHAR) * MAXMSG);
msgID = rxBuf[2];
msgSize = rxBuf[1];
msgData = &rxBuf[3];
switch (msgID)
{
case MESG_RESPONSE_EVENT_ID :
break;
case MESG_CAPABILITIES_ID :
break;
case MESG_BROADCAST_DATA_ID :
Serial.print("Heartrate is ");
Serial.println(msgData[msgSize-1], DEC);
break;
default : Serial.println("ID: Unknown msgID");
}
}
void setup() {
// define pin modes for tx, rx, led pins:
// pinMode(rxPin, INPUT);
// pinMode(txPin, OUTPUT);
pinMode(ledPin, OUTPUT);
// set the data rate for the SoftwareSerial port
mySerial.begin(BAUD);
Serial.begin(9600);
config();
}
void loop()
{
ANT_rxHandler();
}